איך נוכל לעזור לך היום?

Control Expert v16.2 - EULA - Where to find

Product: Control Expert, Unity Pro

Category: Documentation

Issue: Customer Is looking where to find the EULA files

Answer:

The EULA (End User License Agreement) is a

A legal contract between the software provider and the individual user.

Specifies how the software can be used, restrictions, and user responsibilities.

Usually shown during installation and must be accepted to proceed.

If Control Expert is installed on the customer's system, all EULA files can be found in the following directory:

C:\Program Files (x86)\Schneider Electric\License Manager\EULA

Alternatively, the EULA can also be accessed by opening the License Manager or Floating License Manager.

Navigate to the Help menu and select End User License Agreement.

Control Expert License Manager Help- End User License Agreement