המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to Configure Secure Services (HTTPS, SSH, and RADIUS) on SAGE RTU

Title:

How to Configure Secure Services (HTTPS, SSH, and RADIUS) on SAGE RTU

Issue:

Need to enable secure communication and centralized authentication on SAGE RTU for compliance and cybersecurity.

Product:

SAGE Remote Terminal Unit (RTU) All models

Environment:

  • Firmware version C3414-500-S02YZ or later
  • Config@WEB GUI accessible via HTTPS
  • User Manager and Configuration Converter tools installed on PC (.NET Framework 3.5+)

Cause:

Default configuration may allow insecure protocols (HTTP, Telnet, FTP). Secure services must be enabled to meet security standards and prevent unauthorized access.

Resolution:

1.- Enable Secure Services via GUI:

  • Navigate to CPU Configuration → Services Setup.
  • Select the following options for maximum security:
      • HTTPS (Port 443) for encrypted web access
      • SSH Server (Port 22) for secure remote shell
      • SFTP for secure file transfer
      • Enable Remote Shell for VxWorks shell access
      • IPsec for VPN traffic encryption
      • Enable RADIUS Authentication for centralized user management

2.- Configure RADIUS Authentication:

  • Enable RADIUS client in CPU Configuration.
    • Click Configure Servers and enter:
      • IP Address of RADIUS server
      • UDP Port (default 1812)
      • Retries and Timeout values
      • Shared Secret (must match on RTU and RADIUS server)
  • Up to 5 RADIUS servers can be configured.

3.- Generate and Install Keys:

  • SSH: Generate DSA/RSA keys for RTU and users; include in user package via User Manager.
  • HTTPS: Replace default SSL key and certificate using Configuration Converter; generate custom files externally.

4.-Apply Changes:

  • Upload updated configuration via GUI Up/Download tab.
  • Perform RTU reset for changes to take effect.