איך נוכל לעזור לך היום?

EAE - TM262L01MDESE8T - Configuration Assistance w/ EAE v25.0

Issue:

Need to program a M262 dPAC using Automation Expert. Unable to deploy the project in a way that allows access to the inputs and outputs integrated into the main module along with the CPU. Not able to configure the hardware properly.

Product Line:

M262 dPAC controller M262L01MDESE8T.

Resolution:

On a M262 dPAC controller the integrated I/O are disabled and not used, and there is currently no plan to enable them.

This is why these I/O cannot be configured in EcoStruxure Automation Expert.

Into the online help, under the Devices User Guides, the M262 Distributed PAC - User Guide shows in the Presentation of the controller that the I/O terminal connector is not used.

M262 dPAC Presentation

Link to online help:

https://product-help.se.com/EcoStruxure Automation Expert/25.0?lang=en-US&theme=Help

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)