איך נוכל לעזור לך היום?

AR8132A Installation in NetShelter SX Gen 2

Issue: Combination Lock Handle (AR8132A) needs to be installed in NetShelter SX Gen 2 Enclosure

Rack SKU Range: AR3XXXB2 / AR3XXXW2 / AR3XXXSPB2

Cause: Combination Lock Handle is compatible with NetShelter SX Gen 2 with single point lock

Resolution:

Refer to the following instruction and video for detailed steps to install Combination Lock Handle in NetShelter SX Gen 2 Enclosure

1.Before installing the Handle kit, you must remove the front(handle with locking rod) and rear door handles on your rack.
2.Follow the instruction from the Combination Lock Handle instruction manual starting from point 2 in page 2.