איך נוכל לעזור לך היום?

What is the feature of "VLAN Qos Status "in NTSNEC1200 ?

Issue

What is the feature of "VLAN Qos Status "in NTSNEC1200 ?

Product Line

NTSNEC1200

Environment

Edge IO

Resolution

When this feature is activated ,the broadcast and TCP/UDP packets will be tagged with VLAN1 complying with M580 RIO network .

v1