איך נוכל לעזור לך היום?

How many syslog messages could be stored in the local buffer of the BMECRA31310(H) ?

Issue

How many syslog messages could be stored in the local buffer of the BMECRA31310(H) ?

Product Line

M580

Environment

Control Expert 16.2

Resolution

Up to 2048 event messages are stored in the local buffer of the BMECRA31310(H) adapter module. The oldest buffer will be overritted by new arrival events when the buffer is full.