איך נוכל לעזור לך היום?

Does the Edge I/O support RSTP?

Issue:

RSPT with Edge I/O


Product Line:

Edge I/O


Resolution:

The Modicon Edge I/O system does support Rapid Spanning Tree Protocol (RSTP). Key points include:

- RSTP is enabled by default on the system.

- All nodes in an RSTP ring must support RSTP and have it enabled.

- RSTP facilitates quick reconnection during network failures.