איך נוכל לעזור לך היום?

How do I migrate the OFS DA configuration file into the Modicon Communication Server OPCUA for AVEVA System Platform?

Issue:

Migrating the OFS DA configuration file into the Modicon Communication Server(OPCUA) for AVEVA System Platform?


Product Line:

Modicon Communication Server, AVEVA System Platform


Resolution:

You can use the Modicon Communication Server to migrate the configuration of OFS DA to OPC UA devices using the data defined in the configuration file (DeviceConfig.xml) for AVEVA System Platform

Follow these steps to migrate from OFS DA to OPC UA

image1