איך נוכל לעזור לך היום?

How to Power cycle an InRow Cooling Unit Gen2?

PUBLIC

Issue:

How to Power cycle an InRow Cooling Unit Gen2?

Product Line:

InRow Family Gen2.

Environment:

ACRD3XX, ACRC3XX, ACRH3XX, ACRD6XX, ACRC6XX, UNIFLAIR SP,  etc.

Cause:

General aid for Customers

Resolution:

  1. Please click on the home icon (Fig 1) 👇🏻

Image 1

Figure 1

  1. Click on the On/Off button (Fig 2), you might be required to input the pin, use the default one: 1234.

Image 2

Figure 2

  1. Change the state from on to off (Or StandBy), then click OK (Fig 3).

Image 3

Figure 3

  1. When the fans start ramping down, please unplug the dedicated power cord(s) to the unit (It can be top or bottom fed) [Figure 4] or put down the dedicated breaker(s) to the unit (If it’s hard-wired), or if it’s a 600mm InRow (Figure 5) and leave the unit without any power for at least 5 minutes.

Image 4

Figure 4 (For 300mm InRow only).

Image 5

Figure 5 (For 600mm InRow only).

  1. After the 5 min passes, restore the power to the unit, allow a couple of minutes, for the display to pop up, change the mode from Off to On (Figure 3), and test the proper operation of the unit.

NOTE: This process can only be executed from the front display of the unit.