איך נוכל לעזור לך היום?

Is Cascade function available for the ATS490?

Issue:

Does the ATS490 support the Cascade function?

Product Line:

ATS490

Environment:

Multiple motors

Resolution:

The ATS490 does not include a Cascade start function; for this type of application, we recommend using the ATS480 series.