איך נוכל לעזור לך היום?

EcoStruxure process Expert [2025]: How to rectify system start issue happens due to PostGre SQL error

This knowledge base explains the user to troubleshoot the starting of system server error.

As a normal procedure ,user starts the Ecostruxure Process Expert (EPE) SW. It gets stuck with the error as shown in the screenshot below:

IMG_1

After completing the basic checks—such as verifying the firewall settings, restarting the system and confirming that the PostgreSQL port was open, it was observed that the user had allocated only 4 GB of RAM.  Once the RAM allocation was increased to 32 GB, the system server started functioning smoothly.
This is applicable to EcoStruxure Process Expert 2025 only.