איך נוכל לעזור לך היום?

PME - How to move Designer modules into or out of a Grouping Object

Issue

There is a need to move modules onto different windows or pages of the same diagram to organize them.

Product Line

ION Enterprise 5.x

ION Enterprise 6.x

StruxureWare Power Monitoring 7.x

Power Monitoring Expert 7.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Designer

Resolution

Note: These steps are for moving modules within the same Designer node (ION meter or VIP). When copying modules to a different node, review the paste window carefully since a lock paste can unintentionally overwrite existing modules.

1. Select the modules you want to move, then open Edit > Copy:

Edit Copy menu

2. Navigate to the other window of the same Designer node, then open Edit > Paste.

3. Lock paste all modules and select Maintain external inputs. To lock paste all modules, select the first checkbox in the list, press and hold the Shift key, then click the last checkbox in the list.

Green checkbox with lock symbol for all modules, Maintain external inputs checked

4. Click OK. Changes are automatically saved.

Modules successfully moved