איך נוכל לעזור לך היום?

PME - Totalizer or other Arithmetic Module calculation stopped working

Issue

A totalizer or other calculation stopped displaying in Vista/Diagrams or stopped logging. The calculation is from an Arithmetic Module in a VIP, and the output is either stale or n/a:

Output is n/a

Product Line

ION Enterprise 5.x

ION Enterprise 6.x

StruxureWare Power Monitoring 7.x

Power Monitoring Expert 7.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Designer

Cause

There is a communication or configuration problem with either the inputs or a formula in the Setup Registers of the Arithmetic Module.

Resolution

1. Hold Shift + right-click the input to the Arithmetic Module to check for n/a values or communication errors.

Example communication error

2. If one or more inputs show a missing value or have an error:

  • If the input is from a device, either unlink it or resolve the communication issue.
  • If the input is from another module, check the inputs to that module.

3. If the inputs all show a value and no errors are shown, edit the Arithmetic Module and refer to ION Reference to confirm the formulas are configured correctly.

4. If some n/a values are expected or can't be resolved immediately, consider setting N/A Conversion in the Setup Registers of the Arithmetic Module. This will convert n/a inputs to a specific value to allow the calculations to continue working.

n/a conversion option