איך נוכל לעזור לך היום?

Compact DAP212/252/253 to X80 DDM16025 quick wiring - 990XSM00205

Issue

Migrating an ASBDAP212/252/253 to a BMXDDM16025 and need to confirm the 990XSM00205 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

pinout