איך נוכל לעזור לך היום?

EAE25.0: How to show Alias Names of object instances on canvas by default after EAE HMI Start

This knowledge base article will explain users on How to show Alias Names of object instances on canvas by default after EAE HMI Start.

By default the Displaying Alias Names will be in disabled state and we need to enable it  by change the default properties. These settings can be found in General HMI Properties ->Define Values.

HMI

Just we need to make the value TRUE for the System.ToggleAliasDisplayName and select required style of System.DisplayAliasName like Asset tag/HMI Alias/Instance Name as shown in below picture.

display

After performing these settings, Alias Names of all objects shall be displayed in the HMI runtime pages.