איך נוכל לעזור לך היום?

How to replace the Battery Module in APC Smart‑UPS Modular Ultra 5–20 kW?

Issue:
The UPS displays a battery warning or requires battery replacement.

Product Line:
APC Smart‑UPS Modular Ultra 5 kW, 10 kW, 15 kW, and 20 kW

Environment:
UPS Models that begin with SRYL5K up to SRYL20K
All Serial Numbers

Cause:
The replacement battery module (SRYLBM) has failed or reached the end of its service life.

Resolution:
The Smart‑UPS Modular Ultra uses user‑replaceable battery module part number: SRYLBM.
Please review the battery safety information included with this article prior to replacing the battery module.

Battery Replacement Steps:

  • Turn the battery module knob to the OFF position.
  • Loosen the thumb screw by moving it upward or downward, depending on where the battery module is installed.
  • Pull the battery module out of the UPS.
  • Slide the new battery module (SRYLBM) fully into the slot.
  • Tighten the thumb screw to secure the new battery module.
  • Turn the battery module knob to the ON position.

For a visual guide, you can refer to the replacement video below.



If you have any questions or need further assistance, please get in touch with our customer care center at https://www.se.com/us/en/work/support/.

שניידר אלקטריק ישראל

קבצים מצורפים
Battery Safety SRYLBM.pdf [151.56 KB]