איך נוכל לעזור לך היום?

Power Operation Studio Application is Missing

Issue

Power Operation is installed but I am missing Power Operation Studio.

Product Line

Power Scada Operation 2020

Power Scada Operation 2020 R2

Power Scada Operation 2021

Ecostruxure Power Operation 2022

Ecostruxure Power Operation 2024

Environment

Power Operation Studio

Cause

The software was installed as client only rather than a deployment server or a configuration and development environment.


Resolution

Run the applicable product installer, select modify and check off Configuration and Development Environment.