איך נוכל לעזור לך היום?

US version/alternative of the TM251MDESE

-> Issue: Looking for the US alternative of the TM251MDESE

-> Product Line: TM251, Machine Expert

-> Resolution: The TM251MDESE does not have a “US version.” This product is a Modicon M251 dPAC designed exclusively for EcoStruxure Automation Expert. It is not commercially released or supported as a standard PLC in North America, which is why it is not available through normal US distribution channels.

For North America, the TM251MDESE is not interchangeable with a classic M251 PLC, and there is no direct regional substitute for it.

If your application requires a standard Modicon M251 PLC that is fully available and supported in the US, the correct alternative would be a TM251ME series controller (for example, TM251MESE)

If your project specifically requires EcoStruxure Automation Expert, then unfortunately, there's no US variant to suggest.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.If you are not located in North America, please contact your local Customer Care Center for assistance:Support | Schneider Electric Global (se.com)