איך נוכל לעזור לך היום?

Unequal Voltage Readings to Earth on Isolation Transformer Secondary

Question


In Vigilohm IMD‑IT‑S* isolation transformer, when voltage measurements are made between secondary terminals L, N and Protective Earth (PE) they exhibit unequal values.

  • L–PE ≈ higher voltage. Example 170V
  • N–PE ≈ lower voltage. Example 60V
  • L–N ≈ 230 VAC.

Why are the L–PE and N–PE voltages unequal?


Answer


1. Isolation Transformer Principle:

An isolation transformer provides galvanic isolation between its primary and secondary windings. This means there is no direct electrical connection between the secondary circuit and earth (PE). As a result, the secondary side is considered floating with respect to ground.


2. Why “Phantom” Voltages Appear:

Even though the windings are electrically isolated, they are physically close and separated only by insulation. This creates small stray/parasitic capacitances between:

  • Primary and secondary windings.
  • Windings and the transformer core.

Due to these capacitances:

  • A small AC current is capacitively coupled from primary to secondary.
  • When high-impedance digital Multimeter (≈10 MΩ) is used detect this very small leakage current it displays as a voltage.
  • These readings are often referred to as floating or phantom voltages.

3. Reason for Unequal L-PE and N-PE Voltages:

The difference in measured voltages is caused by unequal stray/parasitic capacitances within the transformer:

  • Capacitance values are influenced by winding geometry, position, and proximity to the core
  • The two ends of the secondary winding are not perfectly symmetrical
  • The side with higher capacitive coupling (L) shows a higher voltage relative to earth.
  • The other side (N) shows a lower voltage.

4. Practical Significance of these voltages.

These voltages are not usable energy:

  • They are caused by extremely small leakage currents.
  • They collapse immediately under load.
  • When Low‑impedance Multimeter is used to measure it would read very low or near Zero Voltage.

5. Summary:

  • The observed voltage asymmetry is normal behaviour in floating isolation transformer systems.
  • It is caused by capacitive coupling of the transformer windings, not by a fault.

שניידר אלקטריק ישראל

גלה עוד
מוצר:
גלה עוד
מוצר:
  • תיעוד מוצרים
  • בורר המוצר
  • מוצרים חלופיים והחלפה
  • מרכז עזרה ויצירת קשר
  • איתור סניפי שניידר אלקטריק
  • היכן לקנות
  • הקהילה של Schneider Electric
  • משרות
  • פרופיל חברה
  • דיווח על התנהגות בלתי הולמת
  • נגישות
  • חדר חדשות
  • משקיעים
  • EcoStruxure
  • חיפוש משימה
  • בלוג
  • תנאי ההתקשרות הכלליים
  • מדיניות שמירה על פרטיות
  • הודעה על קובצי Cookie
  • תנאי שימוש
  • Change your cookie settings