איך נוכל לעזור לך היום?

Machine Expert, how can we prevent the controller password to expire?

Issue:

I set up a few of these M241s in the field. Of course, during initial setup I set a login and password.

I noticed that this seems to have expired, requiring me to set a new password. Is there any way to make the password permanent?

Product Line:

Machine Expert version 2.3 and 2.5.

Resolution:

To prevent the expiry of the password to access the controller:

In Machine Expert:

1- From the Device tree, double click on the controller to open the properties and go to the Communication Settings tab.

Communication Settings Tab

2- Click on the Security Settings button to open the following Device Security Settings window.

Device Security Settings

3- Open the CmpUserMgr node.

In it, you will have access to disable the Password Expiration parameter.

User Management parameters

For more details on these parameters consult the online help:

https://product-help.se.com/ESME/2.3/VLP_Software/VLP_Programming/en-US/SoMProg?t=SoMProg/D-SE-0083385.html&theme=ESME

In Machine Expert v2.3 and 2.5, this parameter is enabled by default.

Since version 2.6, it is now disabled by default.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)