איך נוכל לעזור לך היום?

How do I setup Modbus serial communication between two Ecostruxure Machine Expert controllers using the Read_Var function block?

Issue:

How to setup Modbus serial communication between two Ecostruxure Machine Expert controllers using the Read_Var function block


Product Line:

Ecostruxure Machine Expert


Resolution:

In this example, the M251 is setup a Modbus Slave and the M262 as Master. Ensure that both devices serial line settings are identical

image1

Below is the logic where the blink function is used to execute the read every second.  The address table variable of the ADDM block must be used as the address(Addr pin) of the READ_VAR block. Attached is the sample project created in Ecostruxure Machine Expert V2.3

image2

שניידר אלקטריק ישראל

קבצים מצורפים
M262_Master_M251_Slave_Read_Var_Modbus_Serial.project [740.38 KB]