איך נוכל לעזור לך היום?

PME 2024 R3 CM Tool - Backwards Compatibility

Issue

Customer would like to know the compatibility of the PME 2024 R3 CM Tool

Product Line

Power Monitoring Expert 2024 R3

Environment

Software / Upgrade / Migration

Cause

Finding documentation on this specification cannot be found

Resolution

The PME 2024 R3 CM Tool can read from PME systems as far back as PME 7.2. This includes:

Power Monitoring Expert 2024 R1 & R2

Power Monitoring Expert 2023

Power Monitoring Expert 2022

Power Monitoring Expert 2021

Power Monitoring Expert 2020 (9.1)

Power Monitoring Expert 9.0

Power Monitoring Expert 8.X

Power Monitoring Expert 7.2