איך נוכל לעזור לך היום?

How do the ZBZG156 and ZBZM156 lamp test blocks work?

1. What you need to know

A lamp test lets an operator light every pilot light on a panel at once from a single external push button, to check that no light source has failed. The ZBZG156 and ZBZM156 blocks feed the test voltage to each light block through diodes. The choice depends on the light block: ZBZG156 (one diode) for AC/DC LED blocks ZBVJx, ZBVBx and ZBVBGx; ZBZM156 (two diodes) for the 120 V and 230 V ACProtected LED blocks ZBVGx and ZBVMx. Used with ZBVGx or ZBVMx blocks, a ZBZG156 produces only a short light pulse, because of the coupling capacitor at the block input the test then proves nothing.

2. How the lamp test works

Each pilot light keeps it normal control contact. The lamp test adds a second, common supply path from a single test push button to every light block at once.

  • Pressing the test button applies the test voltage to all the pilot lights simultaneously.
  • The diodes in the ZBZ block route that voltage to each light block while keeping the pilot light circuits separated from one another.
  • Releasing the button returns every pilot light to its normal state, so the test button should be a momentary (spring return) operator.
  • The failure mode is silent: a ZBZG156 wired to ZBVGx or ZBVMx blocks does light them - briefly. An operator can read that flash as a passed test.

Titre : ZBZG156 ZBZM156 lamp test wiring diagram - Description : Instruction sheet wiring diagrams for the Harmony lamp test blocks: ZBZG156 on the left for ZBV6, ZBVJ, ZBVB and ZBVBG light blocks; ZBZM156 on the right for ZBVG and ZBVM light blocks.Wiring from the instruction sheet: ZBZG156 on the left, for AC/DC light blocks; ZBZM156 on the right, for 120 V / 230 V AC light blocks.

3. ZBZG156 vs ZBZM156

ZBZG156ZBZM156
ConstructionSingle block - one diodeDouble block - two diodes
Rated voltage12 and 24 V AC/DC, 24-120 V AC/DC48-230 V AC
Compatible light blocksZBVJ- (12 V AC/DC), ZBVBx (24 V AC/DC), ZBVBGx (24-120 V AC/DC), ZBV6x (BA 9s bulb holder)ZBVGx (120 V AC) and ZBVMx (230 V AC), theProtected LED blocks
Result with ZBVG- / ZBVM-A short light pulse only - not a valid lamp testContinuous lighting for as long as the test button is held a valid lamp test
WhyThe coupling capacitor at the input of ZBVGx / ZBVMx blocks limits the lighting time through a single diodeThe two-diode arrangement is designed for these blocks
WiringLeft-hand diagram of the instruction sheetRight-hand diagram of the instruction sheet

4. Schneider Electric references

FunctionReferenceProduct description
Lamp test block - singleZBZG156Single block for the lamp test function, 12 and 24 V AC/DC and 24-120 V AC/DC. One diode.
Lamp test block - doubleZBZM156Double block for the lamp test function, 48-230 V AC. Two diodes. Required for ZBVGx and ZBVMx light blocks.
LED light block, 12 V AC/DCZBVJ3Integral LED light block, green. The last digit sets the colour. Test with ZBZG156.
LED light block, 24 V AC/DCZBVB3Integral LED light block, green. Test with ZBZG156.
LED light block, 24-120 V AC/DCZBVBG3Integral LED light block, green, wide voltage range. Test with ZBZG156.
LED light block, 120 V ACZBVG3""Protected LED" ight block, green, with input coupling capacitor. Test with ZBZM156 only.
LED light block, 230 V ACZBVM3"Protected LED" light block, green, with input coupling capacitor. Test with ZBZM156 only.
Bulb holder, BA 9sZBV6Light block for BA 9s bulb, listed on the instruction sheet as compatible with ZBZG156.

The wiring instruction sheet "ZBZG156, ZBZM156 Wiring test pilot light" is available on both product pages on se.com. Contact Schneider Electric technical support to validate a lamp test circuit mixing several light block types.

שניידר אלקטריק ישראל

קבצים מצורפים
Pilot Light Test Scheme.pdf [17.75 KB]