איך נוכל לעזור לך היום?

How do I customize Single Line Diagram (SLD) labels in EcoSet Design?

EcoSet Design allows users to customize the information displayed on the Single Line Diagram (SLD) through the SLD Labels settings. This feature helps users tailor the displayed information according to project, calculation, or reporting requirements.

How to Configure SLD Labels

  1. Open Settings.
  2. Select the SLD Labels tab.
  3. Create or select an existing custom label template.
  4. Choose the required equipment category from All Entities.
  5. Select the properties to display.
  6. Click Add Selected to include the property in the label.
  7. Arrange the properties in the desired order.
  8. Save the configuration.

The selected properties will be displayed directly on the Single Line Diagram.

labels