איך נוכל לעזור לך היום?

Compact to X80 quick wiring adapter - 990XSM00206

Issue

Migrating the following Compact IO cards to their X80 equivalent and need to confirm the 990XSM00206 quick wiring cable pinout.

AS-BDEP-214 -----> BMXDDI1602/1603

AS-BDEP-216 -----> BMXDDI1602

AS-BDEP-254 -----> BMXDDI1602H/1603H

AS-BDEP-256 -----> BMXDDI1602H

AS-BDEP-257 -----> BMXDDI1604T

AS-BDEP-297 -----> BMXDDI1603

AS-BDEO-216 -----> BMXDDI1602

AS-BDAO-216 -----> BMXDDO1602

AS-BDAP-208 -----> BMXDRA0815

AS-BDAP-258 -----> BMXDRA0815H

AS-BDAP-216 -----> BMXDDO1602

AS-BDAP-256 -----> BMXDDO1602H

AS-BDAP-217 -----> BMXDRA0815H

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

Pinout