איך נוכל לעזור לך היום?

Compact DAP220/250/250C to X80 DDM16022(H) quick wiring - 990XSM00207

Issue

Migrating an ASBDAP220/250/250C to a BMXDDM16022(H) and need to confirm the 990XSM00207 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

pinout