איך נוכל לעזור לך היום?

Compact ADU205 to X80 AMI0410 quick wiring - 990XSM00208

Issue

Migrating an ASBADU205 to a BMXAMI0410 and need to confirm the 990XSM00208 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

pinout