איך נוכל לעזור לך היום?

Compact ADU206/256/210 to X80 AMI0410 quick wiring - 990XSM00210

Issue

Migrating an ASBADU206/256/210 to a BMXAMI0410 and need to confirm the 990XSM00210 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

pinout