Here is the procedure for reset APH parameters. It is only possible with the Graphic display terminal.
- - Enter in the menu Identification 1.11
- - Push enter 2s on the software version of Graphic S.
- - Enter in the menu Diagnostic 1.10
- - Go to "Test procedure" then push enter
- - Go to "RUN Elapsed Time Reset" then push enter
- - Go to "Operating t.reset" then push enter
- - Choose in the list box "Reset kWh" to reset APH.
Released for:Schneider Electric India