Lexium 32 range of servo drive goes into the QUICK STOP under two conditions
- If servo drive meet with an error of class 1 or class 2.
- Upon applying command of QUICK STOP from field bus. QUICK STOP can be triggered by activating bit 3
of “DriveCom Control Word” (DCOMControl)via modbus at an address of 6914 or via CANOpen at address 6040:0 Hex
or via profibus at address of 6914 or via CIP – Common industrial protocol at address 127.1.1
Released for:Schneider Electric India