오늘 무엇을 도와드릴까요?

SFT2841 V10.0 SLOW. When connecting via front face, longer than one minute is required to connect.

Verify that the Win32 Modbus Driver has release version 1.5. Previous and later versions of this driver have resulted in reduced connection speeds. Also, exit the icons that are not associated with the com port that you using. There should only be one icon associated with the Modbus connection. Also, remove active programs which take up processor speed.

AEDL3


  • 1

    Re-published to revised security level: 16 June 2008 by DRM

    Applies to: SFT2841 version V10.0

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188973 V2.0, Originally authored by KBAdPM on 11/08/2007, Last Edited by DaMi on 06/18/2008
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)