Default Webpage Username & Password for PowerLogic Meters and/or their Ethernet Communication Card (ECC)
Issue:
In need of the default webpage username & password for PowerLogic meters with ethernet communication card.
Product Line:
ECC21 (ethernet communication card for CM3000 and CM4000 Series meters)
PM8ECC (ethernet communication card for PM800 Series meters)
PM5500 Series
PM8000 Series
Environment:
Webpage
Resolution
A power meter's webpage can be accessed by entering the meter's designated IP address into a web browser's address bar and logging in with the following default login information.
| Meter | Password |
| CM3000 (ECC21) | admin |
| CM4000 (ECC21) | admin |
Note: ECC21 for CM3000 and CM4000 does not request for username.
Note: To login to the web page of the CM3 and CM4, the Microsoft Silverlight extension must be installed on the web browser. If the webpage does not show menu items and you are using IE 11, please see ECC Web Page does not show menu items. | Schneider Electric USA
| Meter | Username | Password |
| PM800 (PM8ECC) | Administrator | Gateway |
| PM8000 | User1 | 0 |
PM5500 default webpage credentials:
| Configuration area | Username | Default password/passcode | |
| Display passcode | - | 0000 (zero) | |
For Firmware versions:
| Webpages and FTP
| user1 user2 | pass1 pass2 |
For firmware versions:
| Webpages and FTP/FTPS | Administrator | MAC address which is unique for each meter Note: Enter the MAC address of the meter without colon in capital letters. (For example: if the MAC address of the meter is 00:80:f4:02:14:38, then password is 0080F4021438) |
| Webpages | Guest | Powerlogic@1 Note: Forced to change the default password for system security the first time you log in. | |
More Information
Note: the following information applies to the following:
- PM5560 / PM5562 / PM5563 / PM5580 meter models with firmware 2.9.9 and earlier
- PM5570 / PM5660 / PM5760 meter models: 3.2.9 and earlier
- PM5561 meter models: 10.9.9 and earlier
PM5000 series only has web pages for the PM5500 series, and the PM5500 series has two default users with different privileges, Web Master and Product Master.
See Different User Groups for PM5500 series meter and their access level | Schneider Electric USA for more information about account privileges.
The default usernames for the PM5500, user1 and user2, cannot be changed or deleted, but their passwords can be.
The PM5300 does not have a web page even though it has Ethernet communications.
Refer to PM8000 default IP address, username, and password | Schneider Electric USA for more information about the PM8000 username and password.
Please see What are the default User name and Password for the EGX, Link, and Com'X gateway devices? | Schneider Electric USA for information on the default login credentials for web interface on Communication devices i.e. Com'X, Link150, and EGXs