오늘 무엇을 도와드릴까요?

What are the Sepam 40 & 80 firmware requirements for setting up the ACE850TP / ACE850FO

Issue
Want to be able to communicate over TCP/IP and was wondering if the old Sepam in the field has the ability.

Product Line
ACE850TP/ ACE850FO

Resolution
The Sepam 40 and Sepam 80 must have a minimum firmware shown in the below table.
ACE850 (TP/FO)Version OK
Sepam Series 40V7.00 or Greater
Sepam Series 80Base & Application V6.00 or Greater

Note: That the ACE850 cannot be used with the Sepam 20 series.