What is the alternative or replacement of A9A26924 (Obsolete)?
A9A26924 was already obsoleted and replaced by either:
A9A26904 (Standard Application) - Auxiliary contact, Acti9 A9A, iOF, 1 C/O, 100mA to 6A, 24VAC to 415VAC, 24-130 VDC, bottom connection
Datasheet | Instruction Sheet | CAD Files
or
A9A26914 (PLC Application) - Auxiliary contact, Acti9 A9A, iOF, 1 C/O, 2mA to 100mA, 24VAC to 250VAC, 24VDC to 220VDC, bottom connection
Datasheet | Instruction Sheet | CAD Files
For more product substitution, you may refer to the FAQ below:
Singapore: https://www.se.com/sg/en/faqs/FAQ000264549/
Malaysia: https://www.se.com/my/en/faqs/FAQ000264549/
Philippines: https://www.se.com/ph/en/faqs/FAQ000264549/
게시 대상: 슈나이더 일렉트릭 Korea