Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
How to time synchronize PM800 or Sepam series device with PowerLogic SCADA?

You can manually do it following the procedure as per below.

a. You must login with operator2, engineer, administrator or kernel user level.
b. Click on a device list as per below.
Device state

c. Click on Activate from Device Date/Time as per below.
Activate

d. Click on OK

Click ok