Issue
Concept .ASC file can not be imported into Unity Pro.
Product line
Unity Pro, Concept, Control Expert
Resolution
This error can occur when the Concept project was not exported out of the Concept Converter using the first option, "Project with used DFBs".
If "Project with used DFBs (Re-Connect to Equal)" is used the file will not import.
Опубликовано для: Schneider Electric Казахстан