Issue
The attached document is a CIP Modbus Object Read example for a 140NOC77101 using the MBP_MSTR block to read from another Quantum 140NOC77101.
Product Line
Quantum
140NOC77101
Resolution
This program will read from located registers in Schneider PLC's with the following network modules installed:
- 140NOC77101
- BMXNOC0401
- TSXETC101
Do not use this example to read from located registers in Schneider PLC's through the following network module:
- 140NOC78000
Attachments
170NOC77101_CIP_Modbus_Object_READ_Example.pdf
Опубликовано для: Schneider Electric Казахстан