Issue
The attached document is a CIP Modbus Object Write example for a 140NOC77101 using the MBP_MSTR block to write to another Quantum 140NOC77101.
Product Line
Premium TSXETC101
Quantum 140NOC77101
M340 BMXNOC0401
Resolution
This example will write to located registers in Schneider PLC's with the following network modules installed:
- 140NOC77101
- BMXNOC0401
- TSXETC101
This example does not apply writing to located registers in Schneider PLC's through the following network module:
- 140NOC78000
(Removed File URL: 210418_459E/170NOC77101_CIP_Modbus_Object_WRITE_Example.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/357e9bd48a7aadfdc1257afe002cc86c/fl_block_5/0.126?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL210418 V2.0, Originally authored by DaDz on 01/24/2013, Last Edited by DaDz on 01/25/2013
Related ranges: Modicon Quantum
Опубликовано для: Schneider Electric Казахстан