Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Can the E-stop switch on the Magelis XBTGH2460 be replaced with a different type of switch?
Issue
Can the E-Stop switch on the Magelis XBTGH2460 be replaced with a different type of switch?

Product Line
Magelis XBTGH2460

Resolution
No, you can not change the E-Stop button on the Magelis XBTGH2460 to a different type.  It is internally wired for that specific E-Stop and other switch will not function properly.