Issue
Documentation for EGX150 or Link150.
Product Line
EGX150 / Link150
Environment
Brochure, Technical DataSheet, Installation and User Guide, Presentation Overview
Cause
The Link150 gateway serves as an Ethernet coupler for PowerLogic/Schneider Electric system devices and for other communicating devices that use Modbus protocol.
Resolution
The documents attached below include the Brochure, Technical DataSheet, Quick Start Guide, User Guide and Presentation Overview.
Here is a link to the EGX150/Link150 Schneider Electric product information page
EGX150 Declaration of Conformity
Опубликовано для: Schneider Electric Казахстан