These are the part numbers SCADAPACK inter-module cables.
| Part Number | Intermodule cables |
| TBUM297269 | Shielded intermodule cable, 12 inches (0.3m) long |
| TBUM297192 | Shielded intermodule cable, 18 inches (0.45m) long |
| TBUM297193 | Shielded intermodule cable, 24 inches (0.61m) long |
| TBUM297192 | Shielded intermodule cable, 18 inches (0.45m) long |
| TBUM297131 | Shielded intermodule cable, 30 inches (0.76m) long |
| TBUM297162 | Shielded intermodule cable, 45 inches (1.14m) long |
| TBUM297174 | Shielded intermodule cable, 72 inches (1.82m) long |
| TBUM297162 | Shielded intermodule cable, 45 inches (1.14m) long |
Опубликовано для: Schneider Electric Казахстан