Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Cannot find TCP holdoff register in ION 7650
Issue
According to ION Reference (7EN02-0290-09 12/2017) and ION7650 v374 firmware document (7EN12-0297-00 03/2016), a new setup register, called "Modbus TCP Holdoff” was added to the Modbus Master Options module, but it cannot be found.

Product Line
ION 7650

Environment
Designer

Cause
The TCP holdoff register has been moved to a different location.

Resolution
The TCP holdoff register for the ION 7650 can be found in the Ethernet Comm module instead:

Holdoff Register