Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the part number for the locking handle provided on Series E2 MH-style WP enclosures?
Issue:
Need handle and lock for Series E2 MH-WP panelboard NEMA 3R enclosures.

Product Line:
NF and NQ Panelboards

Environment:
Products sold in North America

Resolution:
The following size Nema 3R boxes MH20WP, MH23WP, MH26WP, MH29WP, MH32WP, MH59WP, MH62WP, MH65WP, MH68WP, MH686WP, MH71WP, MH74WP, MH77WP, MH80WP, MH86WP, MH35WP, MH38WP, MH41WP, MH44WP, MH47WP, MH50WP, MH53WP, MH65WP  and MH56WP use the RPLMHWPBAG1 which includes one handle and the mounting hardware to install.