Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Is the SDSA1175 surge suppressor resettable?

Issue:
Is the SDSA1175 surge suppressor resettable?

Product Line:
Surge Protection.

Environment:
Product sold in the United States.

Cause:
Product features

Resolution:
No, there is no manual reset. The LED light should be on if the unit is operational. If the light goes off while the panel power is on, the unit should be replaced.