Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Does 25.8/38kV HVL/cc switchgear require rear access?
Issue:
Rear access for the 25.8/38kV HVL/cc switchgear

Product Line:
HVL/cc Switchgear

Environment:
Products sold in North America

Resolution:
The basic design is Front Access Only, but the overall size makes it difficult to reach C phase (in the rear). This is true for top or bottom cable connections.  It is better if there is rear access for 25.8/38kV HVL/cc switchgear.