Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What plug in unit can be used in place of the SD9352 for the SD busway?
Issue:
Plug in unit that can be used in place of the SD9352

Product Line:
Busway

Environment:
Products sold and used in North America

Resolution:
Plus in units are obsolete for this old series of busway.  The busway will need to be updated to current product.