Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Will an older busway section AP304G10 which is series 1 connect and work with the current product?
Issue:
Connect an older busway section AP304G10 which is series 1 with a current product

Product Line:
Busway

Environment:
Products sold in North America

Cause:
Installation / Setup

Resolution:​​​​​​
Busway Series 4 is the current series, but series 1 will directly connect with the current product.
As long as the part number is the same, the series number does not affect functionality.