Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Is I-Line II busway constructed to be used at 100% of it's rated part number amperage , ie AP2508G10ST for 800A ?
Issue:
Can I Line Busway be operated at 100% of it's listed bus amperage rating ?

Product Line:
Busway

Environment:
I-Line Busway

Resolution:
Yes. The I-Line busway is constructed to allow 100% current flow of bussing amperage listed in the part number.