Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Labels for NF RTI panelboard show voltage rating of 600/347, Is this correct?
Issue:
Why does voltage on NF panelboards show 600Y/347?

Product Line:
Panelboards

Environment:
NF panelboards

Resolution:
Yes,  it is labeled for the maximum voltage that it can be used.  600Y/347 is international voltage not typically used in the US.