Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Can you still get the HVL/cc switch with the removable handle and the push buttons on the front for open and close operation?
Issue:
HVL/cc switch with removable handle and push buttons on the front

Product Line:
Switchboards and Switchgear

Environment:
Medium Voltage Switchgear

Resolution:
Yes, the removable handle is always standard. To get the open and close push buttons the HVL/cc switch must be ordered with the SEM (stored energy mechanism) mechanism. This mechanism has open and closed springs which are pre-charged.